Cart  |  Contact  |  Help  |  auinfo@dwyeromega.com  | 
Toll-Free in Australia: 1800 106 210
International+65 6415 5353

Applications and Benefits of MI Cable in Critical Processes

What is an MI Cable?

Mineral Insulated Cable
Dual OMEGACLADTM Thermocouple Cable
MI cable is a specialized type of cable used in high temperatures or harsh environmental conditions because it has low flammability, even when operating at high temperatures. It resists oxidation and enables precise measurement.

Mineral insulated cable consists of copper or thermocouple wires inside a copper, stainless steel, or Inconel® sheath, insulated by packed minerals such as magnesium oxide (MgO). Magnesium oxide makes an excellent electrical insulation material because it resists oxidation and ionizing radiation, and it is both chemically and physically stable at high temperatures. After the cable has been packed with MgO insulation, it may be rolled under pressure to achieve the desired diameter. The outer sheath protects the internal thermocouple wire from heat, chemical or other environmental damage. The metal sheath may be covered with an additional colored plastic sheath to add in identification and to add an additional layer of protection from corrosion.

An MI cable may contain any number of wires, but the most common configurations include 1, 2 or 3 pairs of conductors. Specialized MI cables may include additional thermocouples in customized configurations. MI cable is available in a variety of diameters and lengths, depending on the specific requirements. Many MI cables are calibrated using sensitive, fast and highly accurate dry block probe calibrators.

RTD and thermocouple sensors manufactured from MI cable are used extensively in heat treating metals, solid waste incinerators, sintering powdered metals, firing ceramic materials, gas or oil fired furnaces, fuel fired heat exchangers, box furnaces, and nuclear or hydrocarbon-based energy plants.

Contact An Expert

Advantages of MI Cable

Molten Metal
Molten Metal
Oil Rig
Oil Rig
The metal sheath that clads MI cable helps to protect the thermocouple wires from oxidation when used in chemically active or wet environments. Corrosion resistance makes MI cable ideal for use in areas where failure and replacement could be dangerous or even impossible. For example, MI cable is used in nuclear plants to monitor core temperatures. It would be extremely dangerous if the temperature controllers were not receiving accurate readings, and it would be difficult to repair or replace cables in that environment.

The mineral fillings in MI cables provide excellent non-reactive insulation, preventing the thermocouple wires from contact with each other or with caustic substances such as oils, solvents or water. This helps to ensure that the thermocouple probes remain accurate, critical in applications such as heat treating or sintering where the quality of the product could be adversely affected by temperature fluctuations.

The insulation in MI cables does not burn, which makes it ideal for applications where fire could be catastrophic. Medical devices, power plants, and oil rigs are examples of places where installation of MI cables makes operations safer.

Since the thermocouple probes are protected from contact with other electrically active wires by the insulation, they are not readily subject to malfunction or inaccurate temperature measurements. Carefully calibrated to meet international standards, MI cables provide accurate and precise temperature measurement over long duty cycles with little or no loss of accuracy.

Because of the mineral insulation, MI cables can operate in high-temperature conditions with no loss of accuracy. This makes them ideal in kilns, firing ceramics or heat treating metals or in any high-temperature process. MI cables retain their accuracy even during and after exposure to high temperatures, so they are ideal as a thermocouple probe in these operations. In addition, for industries such as medical devices or aerospace where safety standards are strictly enforced, process deviations could result in life-threatening quality issues. MI cables are carefully calibrated and verified using NIST standards at Omega against known temperatures or certified thermometers. NIST traceable calibration ensures temperature accuracy under actual operating conditions and provides documentation of their original accuracy. To remain NIST certified, the chain of verification must be intact and the thermocouples must be recalibrated as part of a well-documented and executed quality management system.

Contact An Expert

WHITE PAPER
Download our white paper on
MI Cable
Related topics
RTD Thermocouple Sensors
MI Cable | Tech Reference
What is MI Cable? Comparing Thermocouple Probes Manufactured with MI Cable How to wire RTD sensors and probes | Omega Engineering Preventative vs. Predictive Maintenance | What is the Difference... Preventive vs Predictive Maintenance | Learn the Pros & Cons