Cart  |  Contact  |  Help  |  auinfo@dwyeromega.com  | 
Toll-Free in Australia: 1800 106 210
International+65 6415 5353

Hybrid Ultrasonic Flow Meter Application Helps Ensure Accurate Enzyme Injection

The meter helps accurately monitor flow to ensure accurate enzyme injection

Ultrasonic Flow Meters
Choosing a flow meter is not always a straightforward task. Trial and error sometimes prove to be the only effective method of narrowing down what will work in a particular application. There are several choices, including various invasive and non-invasive solutions to flow monitoring. Paddlewheel, turbine and variable area require direct contact with the fluid, while both mag and ultrasonic meters are non-invasive.

Although paddlewheel and variable area flow meters are more economical, they are not a good choice when the fluid has unknown chemical properties that are abrasive or cause build-up on the unit. A meter without fluid contact proves to be the only solution due to wearing of internal parts, or an impractical maintenance schedule.

Application

URS Div. of URS Corp. provides groundwater remediation services for the Shell Oil Co.’s Carson Terminal in Southern California. The groundwater is contaminated by some unknown bacterial/chemical agent. During the remediation process, the water is pumped through PVC and HDPE pipes, through a series of filters and into a processing chamber where enzymes are injected before being returned to the ground. To be effective, the enzymes must be accurately injected into the water at a rate that is proportional to the water flow rate.

Problem

Accurate measurements of the water flow rate and total flow are critical to the application. Initially, paddlewheel type flow meters had been installed, but a black deposit built up on the paddles required cleaning every two to three days. The paddlewheel meters were replaced with insertion mag meters which failed after one day, as the coating proved to be non-conductive. A turbine meter was tried and failed after only a few hours of operation. A doppler-type ultrasonic meter was tested next, but it failed to give any measurement at all.

A sample of the subject water was sent to a test lab for analysis. The analysis indicated that there were no particles present that could reflect the sound waves, which made Doppler measurements impossible. However, Transit-Time test measurements were successful using a hybrid ultrasonic meter, which can function using either the Doppler or Transit Time measurement methods. The hybrid ultrasonic meter was also able to measure and display the sound speed of the fluid which, due to the contaminants, was significantly different from plain water. Knowledge of the actual fluid sound speed is necessary to properly install and calibrate the meter.

In addition, because of the waters tendency to coat the inside wall of the pipe, which over time also could possibly block the sound waves, the contaminants caused a marked reduction of the sound wave intensity in the groundwater, when compared to clean water. However, the hybrid ultrasonic meter's automatic gain function enabled the meter to function properly over time by increasing and decreasing the sound wave intensity as needed.

Solution

Clamp-on ultrasonic flow meters were successfully installed at the site on 2-in. diameter PVC, and 4-in. diameter HDPE pipes, at multiple measurement points. The ultrasonic Transit Time technology proved to be the low maintenance solution to effectively monitor the URS Div. groundwater remediation process for Shell Oil.

This material has been republished with permission from Blue-White Industries, Ltd.

Related topics
flow level flow meter
Hybrid Ultrasonic Flow Meter | Tech Reference
Hybrid Ultrasonic Flow Meter Helps Accurate Enzyme Injection Flow Measurement in a Return Activated Sludge line Monitoring Water Flow in an Egg Farm Application Technical Learning - OMEGA Engineering® Ultrasonic Level Sensor uses in Cooling Tower Water Basins