Cart  |  Contact  |  Help  |  auinfo@dwyeromega.com  | 
Toll-Free in Australia: 1800 106 210
International+65 6415 5353

Flow Measurement in a Return Activated Sludge Line

Application

Ultrasonic Flow Meters Keene Waste Water Treatment Plant uses a secondary treatment process called activated sludge, a process which converts non-settable substances into a biological floc. This substance is developed in aeration tanks and settled out in final settling tanks. Activated sludge is an aerobic process which promotes the health of microorganisms, ensuring effective treatment. A food and oxygen to microorganism balance must be maintained for optimal treatment. One element of maintaining the biomass requires returning of a portion of the settled sludge from the final settling tanks back to the aeration tanks, keeping the bio system balanced. This portion of the activated sludge is referred to as RAS (Return Activated Sludge). The RAS is returned to the aeration tanks via variable speed centrifugal pumps where accurate flow rate measurement is critical to ensuring a proper ‘food to microorganism’ ratio is maintained. The RAS flow rate is determined by laboratory analysis of the microorganism’s health, the flow rates are adjusted accordingly.

Problem

Keene Waste Water Treatment Plant required flow measurement in a Return Activated Sludge line. Previously, a magnetic flow meter had been selected for the job, however, they were getting a high variance in read out measurements. It was determined that there were stray electrical interference currents causing the inaccurate readings. Due to its failure in accuracy, Keene Waste Water Treatment Plant sought an alternative that could handle the job. Because ultrasonic flow meters only measure sound waves, the electrical interference would not hinder its performance.

Installation & Solution

The treatment facility required reliable flow measurement with 4 to 20 mA output on an existing 18" ductile iron RAS line. The ultrasonic flow meter proved to have all the capacities necessary for the task. Utilizing the mounting harware, installation of the flow meter was completed quickly and easily. With an easy to follow instruction guide, the electronics were configured quickly to accurately measure the flow of the RAS pipe. The ultrasonic flow meter's reliable flow measurement was able to solve the facilities system requirement, without any intrusive equipment, or altering of the existing pipeline.

This material has been republished with permission from Blue-White Industries, Ltd.

Related topics
flow level flow meter
Hybrid Ultrasonic Flow Meters | Tech Reference
Hybrid Ultrasonic Flow Meter Helps Accurate Enzyme Injection Flow Measurement in a Return Activated Sludge line Monitoring Water Flow in an Egg Farm Application Technical Learning - OMEGA Engineering® Ultrasonic Level Sensor uses in Cooling Tower Water Basins